Filter systems

The usage of filters is as diverse as the requirements for their monitoring. The filter of a ventilation system, whose contamination produces a differential pressure of a few millibars, requires different instrumentation than a cartridge filter for oil hydraulics.

All have the requirement for reliability in common, which is also, or especially, true for the measurement technology. Only the reliable measuring signal of a WIKA process transmitter, differential pressure transmitter or pressure gauge enables efficient and trouble-free operation of the system. Your advantage: the energy consumption is optimised and thus also operating costs and environmental compatibility.

Hydraulic filter application

Particles in hydraulic oil lead to a markedly higher wear of all moving parts, such as hydraulic pumps and motors, valve pistons or in the cylinder. Therefore, one or more filters in the circuit are among the most important components. Installation is often in the return line to the tank, where the pressure level is low and the discharge is made against atmospheric pressure. Here a gauge pressure transmitter monitors the filter contamination. If one wants to protect specific components such as the hydraulic motor, then the filter must be fitted in front of these components. For the monitoring of these, one requires differential pressure measurement – measurement of the pressure drop (the contamination) across the filter.

Filter systems
Filter systems

The following 17 products correspond to your selection. You haven't found the product? Please contact us.