Pressure controllers

WIKA pressure controllers: Always the right calibration solution

Pressure controllers are electronic controllers which quickly and automatically provide a pressure based on a supply pressure. Due to the high accuracy and control stability, pressure controllers are especially suitable as references for production lines and laboratories, in order to carry out automatic testing and/or calibration of all types of sensors.
FAQ
FAQ

What is the WIKA Build ID?

The WIKA Build ID is a unique seven-digit code that temporarily saves an individual WIKA instrument configuration. The WIKA configuration can be saved, shared and used later using the Build ID.

What is an air data test set?

An air data test set is a an electronic controller which, based on a supply pressure, automatically provides a pressure at a variable and adjustable rate.

Air data test sets are specifically developed to convert the pressure to be controlled into a ...

more