Contact pressure gauges: Switching and indicating with a single instrument

Wherever the process pressure has to be indicated locally and, at the same time, limit values must be monitored, contact pressure gauges find their application. The switch contacts make or break circuits dependent upon the pointer position of the indicating measuring instrument. If the reading is significantly above or below a set value, they trigger an alarm, hence also the term “alarm contact”. Contact pressure gauges are also suitable for starting, stopping or switching processes.
FAQ
FAQ

What is an isolating amplifier?

The isolating amplifier transmits digital signals from the hazardous area. The signal transmitters can be either sensors per DIN 19234 (NAMUR) or mechanical contacts. The input is securely isolated from the output and the power supply in accordance ...

more