Temperature controllers

Temperature controllers with the latest technology

The compact temperature controllers from WIKA offer display, control and monitoring of temperatures. The configuration of the sensor input is made via the multi-function input. Resistance thermometers, thermocouples and standard industrial signals, such as 4 ... 20 mA, serve as the input variable of a temperature controller. The monitoring output can be set either as relay (for slow control), as logic level for the control of electronic solid-state relays (for fast control and high current loads) or as a continuous 4 ... 20 mA output.
FAQ
FAQ

What is the set point?

The set point is the parameter that the temperature controller should react to. The time required to achieve stable control varies for each controlled system.

What are fluctuations and overshoots?

Two-point control often involves undulation. A temperature rise above the set point, after the start of the temperature control, is referred to as overshoot. Temperature changes around the set point are referred to as fluctuations. A better quality ...

more