Beam load cells

Bending beam and shear beam load cells from WIKA: high precision and stability

Bending beams and load beams are types of force transducers that indirectly measure weight force. Their primary application is in industrial weighing, where the load is static, but beam load cells are also found in machine building and automation, where the load is dynamic. In addition, they are used in laboratories and process industries for indirect torque measurement.

The sensor in most beam load cells is a strain gauge. Bonded to the bending/shear beam, the strain gauge detects the beam’s minute deformation as weight is applied, then converts that data into an output signal. Some shear beams use a thin-film sensor rather than a strain gauge for long-term stability.

WIKA is the only supplier in the field of force measurement that offers beam load cells with thin-film technology. The standardized thin-film sensor is welded into the measuring element using a laser, thereby enabling automated series production. Shear beam load cells with thin-film technology guarantee high quality, excellent temperature characteristics, and precise measurement directly in the force flow. What’s more, WIKA’s beam load cells and other force measuring instruments are engineered and manufactured in central Ohio for fast turnaround times and responsive customer support.