Temperature switches

For each application the right temperature switch

Temperature switches are used in a variety of industrial and technical processes. If a preset temperature is reached, then the temperature switch opens or closes a corresponding switch contact. Depending on the requirements, mechanical or electronic switches can be used. In addition to electronic temperature switches and bimetal temperature switches, WIKA's wide range also includes air velocity meters and frost protection thermostats.
FAQ
FAQ

What happens after the minimum validity of the WIKA Build ID has expired?

Validity cannot be guaranteed after three months.

What is the repeatability with mechanical pressure or temperature switches?

The repeatability is one of the most important performance characteristics for pressure or temperature switches. It describes the maximum deviation between the switch points when repeatedly approaching the same pressure or temperature value. This v ...

more