Mobile fuel cells

On the way to a mobility with reduced CO2 footprint, hydrogen is considered a viable solution, especially for commercial vehicles like for example trucks, buses, municipal vehicles, forklifts or trains. The tank pressure in these vehicles is typically 350 bar with a trend towards the 700 bar standard that is used in passenger cars.

WIKA offers two instruments that are certified in accordance with EC79/2009 and thus provide proof of the sensor's compatibility with the medium hydrogen.

Mobile Fuel Cells
Mobile Fuel Cells

The following 2 products correspond to your selection. You haven't found the product? Please contact us.