Gas density sensors
FAQ
What is the WIKA Build ID?
The WIKA Build ID is a unique seven-digit code that temporarily saves an individual WIKA instrument configuration. The WIKA configuration can be saved, shared and used later using the Build ID.
Can a gas density sensor be damaged if connected to too-high a voltage?
Inadvertent connection of the voltage supply lines to the communication pins of the instrument can cause damage, since the connection pins for the communication have not been designed for high voltages.