Rooftops

Rooftops provide a pleasant feel-good climate in commercial buildings or production and storage halls. The advantage of such a solution is that the system is installed on the roof and doesn’t take up any usable space.

This type of unit can be used either for heating only, cooling only or a combination of both, also in conjunction with a ventilation system.

As these units are installed on the roof of the building, it is important that the equipment and its measuring instruments are able to withstand the ambient conditions.

Air-cooled, roof-mounted systems are extremely energyefficient. The cooling is based on cooling air through the evaporation of water. The energy required for evaporation is extracted from the air, and this therefore cools the air. Electricity is only required for the operation of the fans which circulate the air.

Rooftops × 1

Ambient air

Ambient air
4

Low-pressure line (liquid)

Low-pressure line (liquid)
5

Low-pressure (gas)

Low-pressure (gas)
2

High-pressure line (gas)

High-pressure line (gas)
3

High-pressure line (liquid)

High-pressure line (liquid)
Rooftops
Minimise selection

The following 17 products correspond to your selection. You haven't found the product? Please contact us.