FAQ
Do I need expansion loops?
If you anchor a tubeskin thermocouple outside the furnace (fixed exit) and have any furnace tube movement you will need expansion loops. There are various expansion loops used such as S-loop, multiple coil, single coil and spiral loop.
What is a tubeskin thermocouple?
Tubeskin thermocouples are used for measuring the temperature of tubes in heaters or furnaces. The thermocouple measures the skin temperature of the tube itself.
What benefit does the WIKA Build ID have?
With the ID, the respective planning can be called up again at any time, changed or, in the event of support, further processed and ordered with a WIKA employee. Sharing a configuration is also easier than ever before.