Pressure controllers
FAQ
What is an air data test set?
An air data test set is a an electronic controller which, based on a supply pressure, automatically provides a pressure at a variable and adjustable rate.
Air data test sets are specifically developed to convert the pressure to be controlled into a ...
moreWhat is the WIKA Build ID?
The WIKA Build ID is a unique seven-digit code that temporarily saves an individual WIKA instrument configuration. The WIKA configuration can be saved, shared and used later using the Build ID.