Pressure balances
What is a dead weight tester?
A dead weight tester, also known as a pressure balance, or piston gauge, is a measuring instrument that can be used to determine pressure extremely accurately. As pressure = force/area (p=F/A), a deadweight tester operates on the principle of generating force using physical weights on top of a finely machined piston cylinder system. Pressure balances are used as reference devices for testing, calibrating or adjusting mechanical or electronic measuring instruments. WIKA dead weight testers have a measuring accuracy of 0.05 % up to 0.005 % with measuring ranges from -1 to 6,000 bar. A distinction is made between hydraulic dead weight testers, such as the model CPB5800 and pneumatic dead weight testers, like the model CPB3500.
How does a hydraulic dead weight tester work?
Hydraulic dead weight testers or pressure balances use mineral oil or sebacate oil as the pressure transmission medium.
How does a pneumatic dead weight tester work?
Pneumatic dead weight testers work on the basis of clean, dry, non-corrosive gases, such as air or nitrogen.
How often does a dead weight tester need to be calibrated?
Generally, it is recommended that dead weight testers be calibrated every five years. For more information on mobile calibration service at WIKA, visit the Calibration and Service Center section of our website.
What is the Kn factor?
All piston-cylinder units and masses which can be mounted on DH Budenberg pressure balances are built around a nominal mass-to-pressure conversion coefficient, Kn. The nominal effective area of each piston-cylinder size is such that, under standard ...
moreHow long is the WIKA Build ID valid?
The WIKA Build ID is valid for at least three months.