Level switches

Level switches are important measuring instruments for monitoring the level of liquids in containers. During level measurement, they detect the exact level of the liquid and,when certain switch points are reached, trigger corresponding signals. They are used in various industries to control processes, to monitor stock levels and to ensure plant safety.

WIKA online shop

WIKA online shop

Demand for measuring instruments? Order your standard instruments for level measurement easily and directly from us - with the WIKA quality you are accustomed to.

Where are level switches used?

Level switches are used to monitor liquid levels in containers. They detect switch points and can be used as float switches or level switches. For applications in explosive atmospheres, there are explosion-protected versions, such as, for example, the model OLS-C51 level switch.

How does a level switch with float work?

A level switch detects the liquid level inside of a container. For this purpose, float switches are used, in which the magnet opens or closes one or more reed contacts inside the float, depending on the level. Alternatively, optoelectronic switches are used to monitor the level and detect switch points. Now there are also vibration level switches, which can be found in the WIKA portfolio.

What advantages do level switches offer when monitoring liquids?

Level switches offer a reliable way of monitoring the fill level in containers, thus contributing to safety, efficiency and process monitoring. Due to the precise measurement and detection of switch points, they enable effective control of processes.

What is the difference between a level transmitter and a level switch?

Level transmitters and level switches differ mainly in their functionality and their application area.

Level transmitter Level switches
Function - Continuous measurement of an entire measuring range
- Emits a continuous measuring signal (0 – 100 %)
- Point-based measurement of one or several levels
- Level switch switches as soon as a level is exceeded or dropped below
Range of use - Continuous monitoring of levels in tanks or containers Stopping a process, e.g. filling, or triggering an alarm
- Overflow control
- Dry run protection (e.g. for pumps)

FAQ
FAQ

What benefit does the WIKA Build ID have?

With the ID, the respective planning can be called up again at any time, changed or, in the event of support, further processed and ordered with a WIKA employee. Sharing a configuration is also easier than ever before.