Gas density sensors

Featuring high-accuracy sensor technology and long-term stability

For high-precision online monitoring of the gas density, temperature, pressure and humidity of SF6 gas in internal and external systems of SF6 gas-insulated equipment, WIKA gas density sensors are exceptionally suited. The instruments are notable for their high-accuracy sensor technology which guarantees very good long-term stability and EMC characteristics. Optionally, there are hybrid solutions available which combine gas density transmitters with conventional gas density monitors with switch contacts.

FAQ
FAQ

Where can I find information on the minimum validity of the WIKA Build ID?

The information on the minimum validity of the Build ID is displayed when the ID is generated.

Can a gas density sensor be damaged if connected to too-high a voltage?

Inadvertent connection of the voltage supply lines to the communication pins of the instrument can cause damage, since the connection pins for the communication have not been designed for high voltages.