Submersible pressure sensors

For every hydrostatic level measurement, the right submersible pressure sensor

The submersible pressure transmitter, sometimes also referred to as a level probe, is a specific design of pressure sensor for hydrostatic level measurement in tanks, wells, shafts and bore holes. For this, the submersible pressure transmitter is submerged directly in the liquid to be measured, and positioned as close as possible to the bottom. There, the submersible pressure sensor measures the hydrostatic pressure, which enables a direct conclusion regarding the current level, i.e. the height of the liquid column above it.
FAQ
FAQ

At what pressure could the pressure measuring instrument be destroyed?

Pressure values above the overpressure limit can lead to irreversible damage of the measuring instrument. It does not matter whether this pressure is present constantly or only for a short period of time. In either case, the complete destruction of ...

more

Will a pressure transmitter also work without a power supply?

No.