WIKA

Submersible pressure sensors

For every hydrostatic level measurement, the right submersible pressure sensor

The submersible pressure transmitter, sometimes also referred to as a level probe, is a specific design of pressure sensor for hydrostatic level measurement in tanks, wells, shafts and bore holes. For this, the submersible pressure transmitter is submerged directly in the liquid to be measured, and positioned as close as possible to the bottom. There, the submersible pressure sensor measures the hydrostatic pressure, which enables a direct conclusion regarding the current level, i.e. the height of the liquid column above it.
FAQ
FAQ

Why is the model LS-1000 submersible pressure sensor not available with a cable length of more than 30 m?

The maximum measuring range of the LS-1000 submersible pressure sensor is 1 bar, which corresponds to a submersion depth of 10 m. Experience has shown that customers that have a submersion depth of 10 m typically buy cables with a maximum length of ...

more

How long is the WIKA Build ID valid?

The WIKA Build ID is valid for at least three months.