Gas density sensors

Featuring high-accuracy sensor technology and long-term stability

For high-precision online monitoring of the gas density, temperature, pressure and humidity of SF6 gas in internal and external systems of SF6 gas-insulated equipment, WIKA gas density sensors are exceptionally suited. The instruments are notable for their high-accuracy sensor technology which guarantees very good long-term stability and EMC characteristics. Optionally, there are hybrid solutions available which combine gas density transmitters with conventional gas density monitors with switch contacts.

FAQ
FAQ

What benefit does the WIKA Build ID have?

With the ID, the respective planning can be called up again at any time, changed or, in the event of support, further processed and ordered with a WIKA employee. Sharing a configuration is also easier than ever before.

Can a gas density sensor be damaged if connected incorrectly?

Interchanging the +/- connections cannot damage the instrument, since the connection pins for the voltage supply are protected against reverse polarity.