FAQ
Are there gas density monitors with adjustable contacts?
Gas density monitors usually do not have adjustable contacts. The contacts of the gas density monitors are fixed by a weld after they have been set. This prevents any dangerous operating condition from being caused through unintentional or incorrec ...
moreWhat is the WIKA Build ID?
The WIKA Build ID is a unique seven-digit code that temporarily saves an individual WIKA instrument configuration. The WIKA configuration can be saved, shared and used later using the Build ID.