Pressure measuring

Instruments for pressure measurement by WIKA

In the manufacture of measuring instruments for pressure measurement, WIKA already has over 60 years' experience. We apply our extensive know-how, daily, to the development of our pressure measuring instruments.

Next to temperature, pressure is one of the most important physical state variables. The pressure (p) is defined as a force (F) which acts uniformly over a defined area (A): p=F/A

This force can result from a liquid, from gases or vapours. The International System of Units uses the unit of measurement pascal (Pa) for pressure. In European markets, pressure measurement is generally carried out in 'bar' as a unit, in American markets in 'psi' (to the unit converter).

The following types of pressure are defined:

  • Absolute pressure: Pressure relative to the reference pressure zero (in air-free space).
  • Differential pressure: Difference between two pressures, p1 and p2. Here, the differential pressure p12 is either generated from the pressure element or calculated.
  • Overpressure/gauge pressure: Pressure relative to the atmospheric pressure (ambient pressure).

Mechanical pressure measurement

WIKA offers various types of instruments for mechanical pressure measurement: Pressure gauges with capsule element, diaphragm element or Bourdon tube . With the mechanical pressure measurement with resilient pressure elements, no supply voltage is required. The pressure enters the pressure chamber of the measuring element, of which one or more of the walls deform elastically in proportion to the pressure. This deformation is thus the measure for the pressure. Since the deflection achieved with this is in the range of a few tenths of a millimetre up to 10 millimetres, this deflection is converted into an angle of rotation through a movement. The pressure is read directly off an appropriately divided scale via a pointer.

Electronic pressure measurement

For electronic pressure measurement a sensor is required to detect the pressure and/or its change, and to convert it accurately and repeatably into an electrical signal utilising a physical operating principle. The electrical signal is then a measure of the magnitude of the applied pressure or change in pressure. The instruments for electronic pressure measurement feature excellent dynamic properties and a low material stress, which expresses itself in a high load cycle stability and long-term stability. Measuring instruments for electronic pressure measurement can also be made available in very small sizes, e.g. through the use of semiconductor materials.

FAQ

What is the function of a single-valve block?

With upstream pressure equalising valves it is possible to achieve uniform pressure loading from the plus and minus side, to avoid single-sided overpressure loading during both start-up and operation, and also to enable zero point checks during ope ...

more
FAQ
FAQ

What is the difference between a standard pressure gauge and a safety pattern version?

A safety version (code S3 per EN 837) has an additional solid baffle wall welded between the dial and the measuring system. In addition, the case has a back wall that can blow out completely. The window is typically made of laminated safety glass. ...

more