WIKA

Dial thermometers with scale ranges from -200 to +700 °C

Our dial thermometers work on the bimetal, expansion or gas actuation principle. This enables scale ranges of -200 to +700 °C in different class accuracies, response times and resilience to environmental influences. Diverse connection designs, stem diameters and individual stem lengths enable a flexible measuring location design. Dial thermometers with remote capillaries are particularly versatile. All thermometers are suited for operation in a thermowell if necessary.
FAQ
FAQ

What is the Hall effect?

If a constant current is running through a semiconductor component, and this component is then placed in a magnetic field, then a voltage (Hall voltage) is generated within this semiconductor component which is proportional to the strength of the m ...

more