WIKA ا

Service equipment

Service equipment for installations and corrective maintenance

Filling and handling equipment for SF6 gas are the central tools for the maintenance of gas-insulated equipment. For both installation and maintenance, WIKA supplies the complete product spectrum of efficient service equipment, starting from simple filling carts up to complex, fully automated all-in-one solutions. Furthermore, the instruments support the plant operator with the recording of the SF6 gas volumes and emissions, as is prescribed in the F-gas regulation (EU), No. 517/2014, for specified equipment.

FAQ
FAQ

How long is the WIKA Build ID valid?

The WIKA Build ID is valid for at least three months.

What is the difference between “oil-free” and “oil-less”?

With oil-free, the compressor still contains small amounts of lubricant that could come into the circuit under various circumstances. “Oil-less” refers to compressors that work completely without lubricant.