Portable pressure generation

Simple manual pressure generation

Test pumps serve as pressure generators for the testing, adjustment and calibration of mechanical and electronic pressure measuring instruments through comparative measurements. These pressure tests can take place in the laboratory or workshop, or on-site at the measuring location.
FAQ
FAQ

When is a shut-off valve needed on the CPP1000 - M/L hydraulic test pumps?

When test units with a large internal volumes should be calibrated with it (e.g. pressure gauge from NS 100). For pressure transmitters with a small channel bore volume, a shut-off valve is needed. The volume change of the piston with a complete sp ...

more

How do I get the WIKA Build ID?

In most cases, the WIKA Build ID is available on request. The ID can be requested in all accessible online configurators. The ID can be created in the “Configuration” tab using “Share Configuration”.