Temperature transmitters by WIKA
What is a temperature transmitter?
Temperature transmitters convert the temperature-dependent change in resistance of resistance thermometers or the temperature-dependent change in voltage of thermocouples into a standardised output signal (e.g. 0 ... 10 V or 4 ... 20 mA). With these standardised signals, measured temperature values can be transmitted easily and reliably.
Until the introduction of temperature transmitters, the raw measured values of the sensor were only transmitted to the control room via cable and then converted and processed there. These days, this form of transfer is only used in specific cases, for example, if the ambient temperature is too high or the installation situation is too restricted. For tasks of this type, rail-mounted transmitters also offer a solution. In almost all standard applications, however, head-mounted transmitters have prevailed.
What are the advantages of temperature transmitters?
With the help of a temperature transmitter, not only can users collect measured values digitally via fieldbuses or different protocols, such as HART® or company-specific systems that work parallel to the 4 ... 20 mA output loop, but they can also completely configure the instruments. The relevant elements here are, primarily, the selection of sensor input and measuring range, the storage of measuring location identifiers such as TAG numbers and M&C descriptions as well as the adjustment of the measuring signal by an offset or a specific characteristic curve of the sensor.
A further feature of modern temperature transmitters is the diagnostic functionality: The instrument not only measures the value from the sensor and converts it into the desired temperature unit, it also checks many relevant parameters in the background, e.g. lead resistances, the internal electronics temperature and the supply voltage. If errors occur, the temperature transmitter immediately sends a corresponding signal. In this way, errors such as sensor breaks and short-circuits, effects of the lead and, when using dual sensors, even the drift of a measured value can be detected.
Similar to the different methods of transmission, there are different ways in which the temperature transmitter communicates this information to the distributed control system. In the case of by far the most widespread standardised signal, 4 ... 20 mA, an error is indicated by the current value on the loop being driven high or low. In the case of HART® instruments, a status bit is set at the same time, which then signals a problem. The associated error message can then be read with the corresponding command. With temperature transmitters that operate with one of the fieldbuses, there are many more options for status transmission and for communication between the instrument and the control room.
What does "Pt100" mean?
Pt stands for Platinum with a nominal resistance of 100 Ohm at 0 °C (EN 60751).