WIKA ا

Calibration baths

High reliability and ideal homogeneity

Calibration baths are electronic controllers which automatically, quickly and with the help of a liquid, supply a temperature. Due to the high reliability and exceptional homogeneity in the measuring chamber, calibration baths are particularly suitable as a factory/working standard for the automatic testing and/or calibration of the widest range of temperature probes - independent of diameter. A special micro calibration bath design enables on-site applications.
FAQ
FAQ

How must the inserts be designed in order to get the best results?

The inserts should be drilled in accordance with the diameter of the test items.

In general, the bore diameter, taking the thermal expansion of the test item into account, should be selected to be as small as possible.

Air gap between the thermometer ...

more